Tool/software: Code Composer Studio
Hello,
I am currently executing example program 'led_ex1_blinky.c' from the TMS320F28388D example dual .
i did modify the FLASH link cmd file to load the program in 0x88000 (Sector 4) which was Sector 0 initially after this modification i do not see the controller booting from flash, but works fine when the address is 0x80000. can you let me know if i am missing something to update here.
I have copied the map file data
OUTPUT FILE NAME: <led_ex1_blinky.out>
ENTRY POINT SYMBOL: "code_start" address: 00088000