This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069M: SPI communication problem with 2 different SPI slave devices

Part Number: TMS320F28069M

Hi, 

I have trouble with SPI communication with two different SPI devices. The problem is that one slave needs normal clock phase and the other one needs delayed clock phase, so I need to change clock phase dynamically during program run. 

If I change clock phase during run from NORMAL  to DELAYED , the phase correctly changes to delayed (analyzed on logic analyzator), but when I am trying to change it back to normal phase, then the clock phase remains delayed. 

In conclusion: 

SLAVE1(normal clk phase),  SLAVE2(delayed clk phase) 

Program flow: 


0. Initial SPI setup:  

void HAL_setupSpiA(HAL_Handle handle)
{
  HAL_Obj   *obj = (HAL_Obj *)handle;

  SPI_reset(obj->spiAHandle);
  SPI_setMode(obj->spiAHandle,SPI_Mode_Master);
  SPI_setClkPolarity(obj->spiAHandle,SPI_ClkPolarity_OutputRisingEdge_InputFallingEdge);
  SPI_enableTx(obj->spiAHandle);
  SPI_enableTxFifoEnh(obj->spiAHandle);
  SPI_enableTxFifo(obj->spiAHandle);
  //SPI_setTxDelay(obj->spiAHandle,0x0018);
  SPI_setClkPhase(obj->spiAHandle,SPI_ClkPhase_Normal);
  SPI_setBaudRate(obj->spiAHandle,(SPI_BaudRate_e)(0x000d));  //cca 1,5MHZ
  SPI_setCharLength(obj->spiAHandle,SPI_CharLength_16_Bits);
  SPI_setSuspend(obj->spiAHandle,SPI_TxSuspend_free);
  SPI_enable(obj->spiAHandle);
}

1.  Communication with slave1 OK 

2. Change clock phase to delayed ( SPI_setClkPhase(obj->spiAHandle,SPI_ClkPhase_Delayed) ) 

- phase is correctly changed to delayed

-Communication with SLAVE2 OK 

3. Change clock phase back to normal (SPI_setClkPhase(obj->spiAHandle,SPI_ClkPhase_Normal) ) 

- phase is not changed and remains delayed.

- Communication with SLAVE1 Failed 

Does anyone have any idea how to solve this issue ? 

Thanks for any tip. 

Regards,

Tom.