Part Number: TMS320F28335
Other Parts Discussed in Thread: TMDSCNCD28335
Hi,
how to add External SRAM on F28335 USB Docking Station (TMS320F28335)?
in this post, I understand both F28335 and SRAM are on the same board. When looking at the docking station, some of the GPIOs are not available on J4 - J7 connectors. The idea is to add external memory to the existing docking station.
In TMS320F2833x document there is mentioning of external memory interface (XINTF), and pins GPIO14, GPIO15, GPIO34 have XINTF mentioned in their description.
In post is says "F28335 has an XINTF peripheral that is designed to interface with standard asynchronous SRAMs" and that adding the memory is "relatively seamlessly".
Several questions:
- Are only those three GPIOs (14, 15 and 34) XINTF interface on Docking station with External SRAM?
- In the example from the first post, there are many signals exchanged... Is there a scheme available somewhere and connection diagram for XINTF connection?
- If I want to add external memory, what type and model to use. E.g. IS61WV51216BLL-10TLI has several Address Inputs and Data Inputs/Outputs pins and on F28335 are only three XINTF. Does this mean some other memory is needed?
- When eventually I add the memory, is it automatically recognised or some work is needed? I saw some posts mentioning some Zone 6, Zone 7 configuration/change. I use MATLAB Simulink for coding. The setting possibilities are less compared with Code Composer Studio.
Thank you in advance.