Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, TMDSCNCD28379D
Tool/software: TI C/C++ Compiler
I was trying to use serial_flash_programmer.exe to flash the TI board. Before the flash process, I had set the TI board as the SCI boot mode according to the attached diagram ( GPIO 84 =1, GPIO 72 = 0, TRST = 0). Then, I tried to flash the TI board use the sample text file from f2837xD_fw_upgrade_example folder ( F2837xD_sci_flash_kernels_cpu01.txt and blinky_dc_cpu01.txt). Here is the flash command I had used for flash : serial_flash_programmer.exe -d f2837xD -k F2837xD_sci_flash_kernels_cpu01.txt -a blinky_dc_cpu01.txt -p COM7.
However, the flash progress seems stuck at downloading F2837xD_sci_flash_kernels_cpu01.txt stage (as the second attached image). May I know if anyone meet this situation before ? Thank you.