Part Number: TMS320F28232
I have an SPI bus consisting of one master and two slaves. One of the slaves is an F28232 using McBSP in SPI slave mode. On that particular slave, can I exclusively use SPISTEn (FSX) to select the device? When that device is not selected, and we are talking to the other slave, will it care that the clock is toggling while its SPISTEn (FSX) is not asserted?