Hello
I am using DCL Library V3.3, DCL_PI_CLA structure with DCL_Run_PI_L3 macro.
Can you tell me which method does that library use to implement integration ? (Euler,Trapezoid etc.)
Also, Can you also share the Z-Domain Transfer Function for the Ideal Form Controller
What it seems to me is ; Integration method uses Forward Euler Methode and the Transfer Function is " Kp*(1 + Ki * (1/(z-1)))." Is that accurate ?
Thanks and Regards, İlker.