Part Number: TMS320F28069M
Other Parts Discussed in Thread: MOTORWARE, C2000WARE
Dear team,
I have a similar issue.
I am also trying to implement CAN over motorware.
1 The coding style of motor ware is way different than controlsuit. As the following answer
"You can keep the coding style in controlSUITE or C2000ware to use these CAN example code in motorware, don't need to change it."
So i do not need to change the coding style?
2 Under controlsuit programming, the register of the can module cannot be operated on bits, and shadow registers need to be set for indirect operation.
So after transplanting to motorware, if CAN module programming also carried out the hal programming style, do I still need shadow register operation? If yes, how?
Kindly help me in implementing CAN over motorware.