Part Number: TMS320F28379D
I would like to ask about boot mode pin setting.
I'm checking the manual SPRUHM8I , I want to ask detail information.
We want to use boot-to-flash.
Question
1, At the default setting, GPIO72 and GPIO84 are boot mode pin. If we want to use other GPIO for boot mode pins, How should I set register?
2, If we use other GPIO pins and also these GPIOs are connected nothing, I think that it will boot correctly because GPIO have internal pull-up.
Is that correct?
3, Could you tell me about UI settings when using USER OTP?
4, In case of booting from Flash, is it necessary to assign boot mode pin?
Are there any boot way without boot mode pin setting?
Best regards
Naoki