This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEMU110-U: XDS110 debug probe not working - (Error -1135 @ 0x0) The debug probe reported an error.

Part Number: TMDSEMU110-U
Other Parts Discussed in Thread: TMS320F28069M, MSP432E401Y

I am trying to program a tms320f28069m MCU with the XDS110 debug probe. I have several of these debug probes. I can program the MCU fine with one XDS110, then I try to program the same MCU with a different XDS110 and am getting the mentioned error message. I then try the first XDS110 probe and the MCU programs fine, so it is an issue with the second XDS110.

Things I have tried to resolve this issue:

1. Use the xdsdfu command line tool located in C:\ti\ccs1010\ccs\ccs_base\common\uscif\xds110 to reset the probe. Probe resets, same issue.

2. Use the xdsdfu command line tool located in C:\ti\ccs1010\ccs\ccs_base\common\uscif\xds110 to write firmware firmware_3.0.0.13.bin to the probe. Firmware updates, same issue.

3. Use the xdsdfu command line tool located in C:\ti\ccs1010\ccs\ccs_base\common\uscif\xds110 to ensure configuration 1 is used for programming. Configuration confirmed, same issue.

4. Tried the same USB cable as the working probe, same issue.

5. Tried the same JTAG cable as the working probe, same issue.

I am wondering, is this an issue with the hardware and if so, how can I debug this?