Part Number: TMS320F28379D
Other Parts Discussed in Thread: LAUNCHXL-F28379D, C2000WARE
Hi,
I have a problem with the USB flash programming.
I'm using the development kit launchxl-F28379D and the C2000Ware_3_02_00_00.
By executing the command:
\usb_flash_programmer>usb_flash_programmer.exe -l
I receive the message:
Performing device check only
Error enumerating device interface: 0x0103
This may mean that the device is not attached or the driver is not installed
Error: Couldn't open the USB device
With the CCS 9.3 I don't have problem to program and debug the board.
Any suggestion?
Best Regards,
Luigi