Part Number: TMS320F280049
Other Parts Discussed in Thread: DAC108S085
Tool/software: Code Composer Studio
I have a problem with the DAC108S085. The instruction manual said that the min value of tss is 3-10 ns, and the max value is (1/fSCLK - 3). I use TMS320F280049 to connect this DAC modular, but it's output parameter of tss cannot meet the requirement of the DAC chip.
The output of the tms320f280049 is show below.
SCLK = 1MHz
according to the manual of DAC108S085:
max tss = 997ns
max tsh = 997ns
But in fact the output of TMS320F280049 is
tss = 2000ns
tsh = 480ns
the tss value cannot meet the requirement of DAC
I try to configure the output of the DSP, but I cannot find the way to configure this parameter of DSP