Hi Expert,
My customer using 100pin F28075, set GPIO29&28 as SCI boot pin to boot load from extern ARM device at first time, refer to the below thread method.
http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/890085/3297264#3297264
After updated the code to device, they'd like the code booted from Flash at next time which resetting the device and changing the GPIO29&28 to high level.
However, they have a trouble to achieve Flash boot load mode, after changed the OTP area as above e2e thread suggested. Because the code would read the OTP content and change to SCI boot mode, though the GPIO29&28 is high.
They'd like to check if the boot load mode be changed from SCI to Flash? If yes, could you please help to give the guides/notes to achieve it? Thanks!
Best Regards
Rayna Wang