Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: UNIFLASH, MOTORWARE, TMS320F28035, LAUNCHXL-F28069M, CONTROLSUITE, DRV8312, INSTASPIN-BLDC
Tool/software: TI C/C++ Compiler
Hello,
we have a DRV8312-69M-KIT (2019) and for that we have installed and configured to work properly, MatLab 2019a, CCS 6.2 and UniFlash 4.1. Taking the example c28069pmsmfoc_ert.slx and building (compiling), it is generating a c28069pmsmfoc_ert.out, which is loaded easily in DRV8312-69M-KIT by using UniFlash 4.1 app. Also, it is possible to compile any Lab project given in MotorWare app by using CCS 6.2
Last month (Nov. 2020) we have bought a DRV8312-C2-KIT and we have tried to put it working with the same software (MatLab 2019a, etc.) but it is impossible. We have downloaded the new version of TI C2000 Piccolo Support from Embedded Coder and also Concerto version, but we have not found c28035pmsmfoc_ert.slx in this package. Where is the examples for DRV8312-C2-KIT?
On the other hand, we have compiled a simple Simulink diagram with Digital Output for 28035 and it can not loaded in DRV8312-C2-KIT by using UniFlash 4.1, while the same version for 28069 loads properly. It seems that the problem is due to the USB (JTAG) interface. For 28069 UniFlash uses XDS 100 v2 and for 28035 it is not valid, being valid XDS 100 v1 (according to TI web, DRV8312-C2-KIT info). The problem is that UniFlash 4.1 does not support XDS 100 v1, neither UniFlash 6.1. Perhaps the solution could be to configure v2 as v1, if somebody knows how to do?
Then, please, somebody could help me saying how versions of MatLab, TI C2000 Support, CCS and UniFlash are neccesary to work easily for DRV8312-C2-KIT and DRV8312-69M-KIT at the same time.
Thank you very much!
Patxi