This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28377S: CCS6.1.0

Part Number: TMS320F28377S

Tool/software: Code Composer Studio

My question is: how can I make the On-Chip flash option in the tools menu work so that I can enter a preset password? When the password of the Target has been activated, how can I enter the debug session?

The PC running ccs6.1.0 has established physical connection with the target through XDS100. The Connect Target in the Run menu is gray. If the Target’s password has been activated, ccs6.1.0 will display an error when debug is selected or press F11 and cannot continue. Only when the password in the Target is not activated, select Debug or press F11 to successfully enter the debug session, and the On-Chip flash option in the Tools menu is valid.

The following is the screenshots after opening ccs6.1.0.

If the password of the Target is not activated, press the debug button to enter the following state:

If the Target’s password has been activated, ccs6.1.0 will display an error when debug is selected or press F11:

Click OK to enter the following state: