This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS / TMDSCNCD28388D:Use of C2000 ware routine

Part Number: TMDSCNCD28388D
Other Parts Discussed in Thread: C2000WARE

Tool/software: Code Composer Studio

The routine EtherCAT in C2000 ware is used_ slave_ cpu1_ hal.c.
In ccs10.0 software, there is an error when compiling.

然后,跟着文件EtherCAT Slave Controller Software  USER’S GUIDE,一步步的进行。突然有个.exe,找不到在哪。

Then, follow the file EtherCAT slave controller software user's guide step by step. All of a sudden, there's an. Exe. I can't find it.

特来请教一下,是否有针对此例程的测试视频步骤教学。不止这个地方有问题,SSC  Tool v5.12的软件在使用的过程中,搜索设备,只能搜索到device1.

Especially to ask if there is a test video step teaching for this routine. More than that, SSC tool v5.12 software in the process of using, search device, can only search device 1

有的话,应该去哪找呢

If so, where should I look

感谢

thanks.