Hi,
For FSI, if daisy-chain is used, what will be the limitaion for the node devices? My point of view, there's no limitation.
If 100 bytes are needed to be transmited to each device, 7 times frame transmit activities are needed, as each time max data is 16 words. Is that right?
With 100Mbps, what will be the total latency for 100 bytes transmit, from the first frame transmit, to the 7th frame received at node device No.50 (just an example)?
Thanks a lot.
Br, Jordan