Other Parts Discussed in Thread: TMS320F28388D
rt Number: TMS320F28388D
Hello Experts,
I just wanted to get a confirmation from you on the timing analysis done based on the Prescaler and Pre-Divider for the Watchdog clock. Attached the excel sheet used for the Watcdog clock configuration.xlsxcalculation
please let me know if my assumption is correct.
Per the calculation, I believe the calculated time is the watchdog time out value before which it needs to be refreshed.
| . Prescalar PreDivider . |
0 | 1 | 2 | 3 | 4 | 5 | 6 | 7 |
| 0 | 51.20E-06 | 51.20E-06 | 01.02E-04 | 02.05E-04 | 04.10E-04 | 08.19E-04 | 16.38E-04 | 32.77E-04 |
| 1 | 01.02E-04 | 01.02E-04 | 02.05E-04 | 04.10E-04 | 08.19E-04 | 16.38E-04 | 32.77E-04 | 65.54E-04 |
| 2 | 02.05E-04 | 02.05E-04 | 04.10E-04 | 08.19E-04 | 16.38E-04 | 32.77E-04 | 65.54E-04 | 01.31E-02 |
| 3 | 04.10E-04 | 04.10E-04 | 08.19E-04 | 16.38E-04 | 32.77E-04 | 65.54E-04 | 01.31E-02 | 02.62E-02 |
| 8 | 20.00E-08 | 20.00E-08 | 40.00E-08 | 80.00E-08 | 01.60E-06 | 03.20E-06 | 06.40E-06 | 12.80E-06 |
| 9 | 40.00E-08 | 40.00E-08 | 80.00E-08 | 01.60E-06 | 03.20E-06 | 06.40E-06 | 12.80E-06 | 25.60E-06 |
| 10 | 80.00E-08 | 80.00E-08 | 01.60E-06 | 03.20E-06 | 06.40E-06 | 12.80E-06 | 25.60E-06 | 51.20E-06 |
| 11 | 01.60E-06 | 01.60E-06 | 03.20E-06 | 06.40E-06 | 12.80E-06 | 25.60E-06 | 51.20E-06 | 01.02E-04 |
| 12 | 03.20E-06 | 03.20E-06 | 06.40E-06 | 12.80E-06 | 25.60E-06 | 51.20E-06 | 01.02E-04 | 02.05E-04 |
| 13 | 06.40E-06 | 06.40E-06 | 12.80E-06 | 25.60E-06 | 51.20E-06 | 01.02E-04 | 02.05E-04 | 04.10E-04 |
| 14 | 12.80E-06 | 12.80E-06 | 25.60E-06 | 51.20E-06 | 01.02E-04 | 02.05E-04 | 04.10E-04 | 08.19E-04 |
| 15 | 25.60E-06 | 25.60E-06 | 51.20E-06 | 01.02E-04 | 02.05E-04 | 04.10E-04 | 08.19E-04 | 16.38E-04 |
Regards,
Mohan