Part Number: TMS320F28377D
Other Parts Discussed in Thread: SYSCONFIG
Hi,
I want to use the CLB tool to generate a customised ePWM signal using ePWM internal peripherals of PWM1 and PWM2 and apply the following logic in a TIEL to produce PWM3A and PWM3B at pins GPIO4 and GPIO5 by using CLB overriding option.
(PWM3A= PWM1A XOR PWM2A ), and (PWM3B =PWM1B NXOR PWM2B )
I modified the clb_ex8_external_signal_AND_gate CLB example and inserted a few additional codes to generate PWM1 and PWM2 signals as global signals.
However, I don't get the signals I am looking for. So please advice me?
#include "driverlib.h"
#include "device.h"
#include "clb_config.h"
#include "clb.h"
#include "board.h"
#include "F28x_Project.h"
void InitEPwm1(void); // Init ePWM module 1
void InitEPwm2(void);
void main(void)
{
Device_init();
Device_initGPIO();
Interrupt_initModule();
Interrupt_initVectorTable();
InitEPwm1(); //
InitEPwm2(); //
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM3);
Board_init();
initTILE1(myCLB0_BASE);
CLB_enableCLB(myCLB0_BASE);
while(1)
{
asm(" NOP");
}
}
void InitEPwm1(void)
{
EPwm1Regs.TBPRD = 450; // Period = 900 TBCLK counts
EPwm1Regs.TBPHS.bit.TBPHS = 0; // Set Phase register to zero
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetrical mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Master module
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
EPwm1Regs.CMPA.bit.CMPA= 285; // adjust duty for output EPWM1A
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM1A
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi complementary
EPwm1Regs.DBRED.bit.DBRED = 20; // Dead-Band Generator Rising Edge Delay Count Register
EPwm1Regs.DBFED.bit.DBFED = 20; // Dead-Band Generator Falling Edge Delay Count Register
}
//------------------------------------------------------------------------------------------
void InitEPwm2(void)
{
EPwm2Regs.TBPRD = 450; // Period = 900 TBCLK counts
EPwm2Regs.TBPHS.bit.TBPHS = 300; // Phase = 300/900 * 360 = 120 deg
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Symmetrical mode
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Slave module
EPwm2Regs.TBCTL.bit.PHSDIR = TB_DOWN; // Count DOWN on sync (=120 deg)
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through
EPwm2Regs.CMPA.bit.CMPA = 285; // adjust duty for output EPWM2A
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // load on CTR=Zero
EPwm2Regs.AQCTLA.bit.CAU = AQ_SET; // set actions for EPWM2A
EPwm2Regs.AQCTLA.bit.CAD = AQ_CLEAR;
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; // enable Dead-band module
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; // Active Hi Complementary
EPwm2Regs.DBRED.bit.DBRED = 20; // Dead-Band Generator Rising Edge Delay Count Register
EPwm2Regs.DBFED.bit.DBFED = 20; // Dead-Band Generator Falling Edge Delay Count Register
}