Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
I have checked out many threads regarding upgrading the firmware of the TMS320F28388D and I know that so far there are no "ّFlash Kernel" and "Flash API" for this chip. We would like to do Live Firmware Update for this chip about which I have two questions:
1) Are there any alternative solutions to upgrade the firmware? Even if we could only update CPU1 and CPU2 (without the Cortex-M4) that should still suffice.
2) If there are no Flash Kernel and API for TMS320F28388D, then how does JTAG is able to program the chip? Can we implement whatever method JTAG is using?
Regards