Part Number: TMS320F28388D
Other Parts Discussed in Thread: ADS8365, C2000WARE
Hi,
I am using an external memory interface(EMIF) to interface the external ADC (ADS8365) using Asynchronous memory configuration.
I am reading the data to the EMIF memory region(EMIF1 CS2n - Program + Data 2M x 16 : 0x0010 0000 to 0x002F FFFF) by configuring the read strobe, hold and setup timing parameters.
I referred to the section: 12.6.2.2.1 Asynchronous 1 Configuration Register (ASYNC_CS2_CFG) Settings for EMIF to LH28F800BJE-PTTL90 Interface from TRM and accordingly set the corresponding read time according to the XADC timing characteristics.
One thing I am not sure about is how to read could be performed as both the modules have different operating frequencies, i:e; emif it is 200mhz and xadc is max. 5mhz.
Can we pull down the emif to lower frequency? As i am unable to read the data while configuring the peripheral properly.
Please note, we have not configured the strobe mode, and EM1DQM pin as well.
I have also attached the emif timing characteristic sheet to update the ASYNC_CS2_CR values.
Kindly please check and revert asap.
Regards
Gurusha