Part Number: TMS320F280049
HI,
I would like to use the configurable logic for this device but am not sure which GPIOs can be configured for this. Are there certain GPIOs or can all the GPIOs be connected to the CLB if needed?
Thanks,
Jose
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
HI,
I would like to use the configurable logic for this device but am not sure which GPIOs can be configured for this. Are there certain GPIOs or can all the GPIOs be connected to the CLB if needed?
Thanks,
Jose
For this devices, you can override existing peripheral outputs such as EPWM. So where the EPWM1-4 outputs are connected to on the GPIO.
Also the CLBx_OUT4 and OUT5 are connected to the OUTPUT XBAR. So they can be connected to GPIO through that!
Check out this document: https://www.ti.com/lit/an/spracl3/spracl3.pdf?ts=1616186795647&ref_url=https%253A%252F%252Ftraining.ti.com%252F
That has a section on the connections.
Nima