Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Hi,
F28377D load CPU2 flash kernel to GS RAM, then use IPC_BRANCH call command so that CPU2 start executing code from the entry point of GS RAM.
Now my customer is using F28388D.
the IPC boot commands are different and I don't see IPC branch command(to GS RAM) in F28388D TRM.
(1) Can I use the F28388D IPC command to achieve the boot CPU2 and CM ?
(2) I think one solution is to use "IPC Message Copy to RAM Boot" instead of (1) .
However, Message RAM has only 2KB, which is not enough.
Is there any solution?
Thanks,
Koki