This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28034: some questions about IEC60730

Part Number: TMS320F28034
Other Parts Discussed in Thread: C2000WARE,

Hi Expert,

My customer are do the certification of IEC60730, and 3rd party have some question as attached, would you help answer the question below? for more details, refer to the attached.

Question 1there are a lot of Core Registers that from CCS windowswhy STL_CPU_TEST only cover part of CPU core register? Any document to talk if these are not safety related ?

Question 2there are OSC1 and OSC2 two clock source, is these two clock independentany document to introduce

Question 3PSA CRC is hardware module or software module

question list for IEC60730.docx

  • 1. Can you clarify which ones you're talking about? PC is covered by another module in the library. It is true that ST1 and RPC are missing. I wrote tests for these in the F28004x port of this test that could be added to the F2803x version. If you have a newer version of C2000Ware installed, take a look at C2000Ware\libraries\diagnostic\f28004x\source\stl_cpu_reg.asm.

    If this question is referring to STF, RxL, and RxH registers, those are all part of the FPU--which if I recall correctly doesn't actually apply to this device.

    2. They are separate internal oscillators if that's what you mean by independent. I think the TRM is the primary place that documents the oscillators and their uses.

    3. The PSA is hardware.

    Whitney

  • Hi Whitney,

    Thanks for your reply!

    for question #3, 3rd party think that hardware for CRC is not reliable, they think CRC should be done all by software, do we have any further material to prove that PSA for CRC is compliance with IEC60730?

  • Hi Strong,

    I'm out of the office today and tomorrow, but I'll investigate and get back to you next week.

    Whitney

  • Strong,

    There are links to the safety manual and VDE certification on the TMS320F28034 product page.

    Whitney