This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Memory allocation error.

Part Number: TMS320F28379D

HI,

I am getting the error that "program will not fit into available memory, or the section contains a call
site that requires a trampoline that can't be generated for this section.
placement with alignment/blocking fails for section ".text" size 0x1f89page". 

I have tried to allocate the unused memory of Page 1 to the .text memory in the page 0. It didn't help.

Then, I tried to comment a big portion of the program which leads to the successful compilation but in the memory allocation view, it is showing that 99% of all the EPWM modules and CPUsysregs memory used. Even though I am using only EPWM1 module. Please help.