This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069F: InstaSPIN-FOC Lab project : Lab11a: floating point support with the fpu32 enabled

Part Number: TMS320F28069F
Other Parts Discussed in Thread: MOTORWARE

Hello,

I have a question on an InstaSPIN-FOC Lab project in motorware.

Particularly it is on Lab11a.

It seems that lab11a does not use the fpu32 available on the 28069 device; instead it uses the softlib for the floating point support.

However I plan to use the fpu32 for the lab11a.

I have noticed that lab10a uses the softlib for the floating point support, whereas lab10c uses the fpu32 for the floating point support.

Therefore, may I create the lab11c CCS project from the lab11a project in a similar way as the lab10c CCS project is created from the lab10a project?

Thank you for your guidance.

With regards,

JS Yoo

  • Yes, you can refer to lab10c to use the fpu32, but I don't think it's necessary to do this for motor control, The IQmath based project should have the same performance as using floating-point.