Part Number: TMS320F280049
Hello there,
I already asked related question regarding using HRCAP for precise frequency measurement here.
I would like to compare these three modules (HRCAP, eCAP, eQEP) for frequency measurement of square wave.
Lets say we have square wave of 50% duty cycle running at 1-2 MHz. Width of each pulse is dependent on frequency as: 0.25 usec (50% duty cycle of 2 MHz) to 0.5 usec (50% duty cycle of 1 MHz).
Please see following picture showing measured signal:

My questions:
Q1: Can each of these modules be used for measurement of such a signal?
Q2: What are limitations of each module in matter of min and max input frequency, duty cycle etc.?
Q3: What are achievable timing resolutions for each module?
For eCAP I found in SPRAAH1 and SPRU807B where timing resolution for eCAP is 1/SYSCLKOUT. Is then correct that eCAP has timing resolution of 10ns at 100MHz SYSCLK?
For HRCAP I found in SPRS945F (7.11.2.1) timing resolution of 450 ps for measurement longer >5usec.
For eQEP I found SPRSP14D (7.12.4.1) where timing resolution is specified as 2x SYSCLK. Here I am not sure what is resolution then.
Can you please summarize input frequencies requirements for each of this module?
I appreciate your help.
Thank you,
Michael