This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28069M: NEED information regarding how to use ePWM block

Part Number: LAUNCHXL-F28069M
Other Parts Discussed in Thread: C2000WARE

Hi TI expert

I have below questions, Could you please reply to this.

1. For the F28069M launchpad clock frequency is 90 MHz. So what is the maximum switching frequency we can use for generating PWM pulse? is there any limitation?

2.If I am generating any PWM pulse using some logic in Simulink can we directly apply the same PWM pulse to the EPWM block to generate the pulse and apply it to the hardware .is yes there please provide the process if no then pls mention the alternative process.

Best regards,

Thomas