Hello,
I am using the TMS320F28377S and it seems to be held in reset. I am able to connect to the device though the XDS110 debug probe and start my program, but on power cycle, the MCU does not run. It seems that the TRST overrides whatever my issue is.
The /XRS pin is at 3.3V. I have disabled my watchdog reset and the problem persists.
Any input is appreciated.
Thanks,
Cameron