Part Number: TMS320F280049
While using the serial flash programmer I encountered a problem loading the kernel file onto the ram. After two hex digits the download on the HW stops as seen in the picture. Does anyone know what to do about it ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049
While using the serial flash programmer I encountered a problem loading the kernel file onto the ram. After two hex digits the download on the HW stops as seen in the picture. Does anyone know what to do about it ?
Hi Sal,
thanks for your reply, unfortunately after I resolved the issue with the kernel file I encountered another Problem.
I followed your instructions and recompiled the kernel file. I am now able to download the kernel file onto the ram. Now I tried to load an application file onto the devices flash with the use of option 1-DFU. The application returns a NACK Error (see picture below). Is there someting that I did wrong ? I already lowered the baud rate but that didnt help.
Best regards,
Patrick
German Aerospace Center
If it cannot get past the autobaud lock, that makes me think there is something wrong with the connection to the pins that the SCI is using.
Which pins are you using? How are you connecting to them?
Also, which board are you using? controlCARD?
Regards,
sal