Part Number: TMS320F280049
Other Parts Discussed in Thread: C2000WARE
Hi,
I'm testing the serial flash programming function for my customer. I tested with "flashapi_ex2_sci_kernel.txt" in C2000ware,
the directory is C:\ti\c2000\C2000Ware_1_00_02_00\utilities\flash_programmers\serial_flash_programmer\f28004x_fw_upgrade_example.
I can download the flash kernel to RAM through SCI bootloader, but when I command to erase or upgrade the application project, there will be error.
The error when I try to erase the flash is shown as below. What does the error mean? How can I fix it?