Part Number: TMS320LF2407A
Tool/software: Code Composer Studio
As per this post:
I have the same issue I have a board that is unsupported and have a TMX320LF2407A IC with a JTAG header. I have bought a XDS510LC from spectrum digital. I have downloaded CCS3.3 and I can connect to the controller using JTAG. I can run and stop the processor thus my connection is ok.
I want to copy the data from this IC using JTAG and CCS and then allow me to place it onto another board for repair. Is this possible?
The previous post people say: save the flash contents as a COFF file (.out file).
Problem is that I have never used CCS so have no idea. Someone else said: "You need a working copy of CCS3.3 on a PC and a debug probe like XDS510PP+. If you have these, then you could connect to the device via JTAG and easily dump the flash contents."
Easily dump the flash contents. Can anyone help?! What do I need to do step by step on CCS3.3 in order to get this code. Once I have this then I also need to know how to write it.
thanks