This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: About HET5A Boot Time Software Test of Function Using I/O Loopback

Part Number: TMS570LS3137


I use TMS570LS3137.

I have a question about how to implement "Boot Time Software Test of Function Using I / O Loopback".

· Does Analog Loopback recognize using the Digital Loopback function because signals may be output from the pins and other ICs may be damaged?
· In the case of digital loopback, if both pairs are output, it is better to switch the output and try each loopback
· At the time of loop back, is it necessary to wait between writing and reading?

  • Hello,

    The various loopback operation modes are defined in detail within the Technical reference manual in section 20.2.5.7.

    user4777395 said:
    · Does Analog Loopback recognize using the Digital Loopback function because signals may be output from the pins and other ICs may be damaged?

    Essentially, in analog mode, the signal has to cross outside the boundary of the logic into the analog input and output buffers to test the full path of the signal where as a digital loopback does not go outside the digital logic of the device. If only digital loopback is used, it is possible to miss faults within the buffer structures or even issues resulting from shorted circuits outside the device since it will pick up the signals on the pins.

    user4777395 said:
    · In the case of digital loopback, if both pairs are output, it is better to switch the output and try each loopback

    Note that the test of function at boot time doesn't have to be your final N2HET program so IO directions can be changed through loading and reloading different test versions in the HET program memory. Your primary concern is to look for latent faults including shorts/opens and stuck at faults dependent on your system capability. If there are concerns with damage to an external component, then this should be considered in the design of the test and noted as a limitation on due to the system implementation.

    user4777395 said:
    · At the time of loop back, is it necessary to wait between writing and reading?

    Generally, there could be some latency but I haven't seen this arising as an issue previously.

  • Hi Chuck.

    > Essentially, in analog mode, the signal in the analog input and output buffers to test the full path of the signal where a digital loopback does not go outside the digital logic of the device.

    >Only digital loopback is used, it is possible to miss faults within the buffer structures or even issues derived from outside devices outside the devices will it will pick up the signals on the pins.

    Analog loopback is a recognition that needs to make a loopback circuit.
    On this circuit design, it is difficult to make a loopback circuit.
    In this case, there is another detection method for the fault that was supposed to be detected by analog loopback?


    > Note that the test of function at boot time N2HET program so IO directions can be changed through loading and reloading different test versions in the HET program memory.

    I'm sorry for not knowing this.

    Boot Time Software Test of Function Using I / O Loopback was recognized by register manipulation, is it using HET Code?

  • Analog loopback is a recognition that needs to make a loopback circuit.
    On this circuit design, it is difficult to make a loopback circuit.
    In this case, there is another detection method for the fault that was supposed to be detected by analog loopback?

    This is not a true statement. When using analog loop back it is not necessary to make a physical loop back circuit in your design/PCB. The Analog loop back still is done within the boundaries of the device. The difference is that it is outside the boundaries of the digital logic for the module. For clarity, consider the diagram below.

    Note in the diagram that the area shown as 'A' is the digital logic part of the module, the area indicated as 'B' is the analog buffers for taking the digital signals out to the real world (still inside the chip), and the area indicated as 'C' is outside the chip or at the pin level of the device. Note the different paths for checking the IO paths. Specifically, note the difference in the boundaries that are crossed and which of the analog buffers are exercised.

    > Note that the test of function at boot time N2HET program so IO directions can be changed through loading and reloading different test versions in the HET program memory.

    I'm sorry for not knowing this.

    It seems my message here is a little confusing because some autocorrect changes that were made. My intent was to state that if you are checking HET IOMM changes, it isn't mandatory that you use the same HET program for testing that you use in your application. The goal of the IOMM loopback test is to insure the correct input and output buffers are connected to the digital logic of the module in use (HET in this case). You could do some simple GIO use of the HET pin to prove that you can toggle the outputs and read the inputs through the HE digital logic/registers.

    Boot Time Software Test of Function Using I / O Loopback was recognized by register manipulation, is it using HET Code?

    I am not certain what you are asking here but I believe you are driving at a question of how to implement the loopback at the register level? So each module will have the loop back capability as defined in the TRM. In some cases there is no specific loop back functionality defined and is inherent in the design of the IO buffers. For example, to test a GPIO functionally, you need only to set the direction to output, drive the output high and low and read the input in the input register to see the corresponding changes from the input buffers. For other IP, it might be necessary to accommodate system level tests to check the paths and functions. It really is a situation where you need to understand the operation of the module on the chip and how it fits within the system application to decide the best way to assure proper operation and balance that with overall system performance needs.

  • Thank you.
    Thanks to the figure I understood the difference between analog and digital.

    In this system, HET is planning to use PWM output using HET Code instead of IO.
    In this case, what should I do as a loopback test?

  • Hello,

    Analog loop back is described in detail in the TRM so I would first suggest that you review the information there. The manual is located at http://www.ti.com/litv/pdf/spnu499b. The specific section is section describing loop back mode is "20.2.5.7 Loop Back Mode."

    Once you have a chance to review it, please come back if there are any questions. If the material answers your question, please mark the answer here verified so the thread can be closed. Thanks!