Part Number: TMS570LS0432
Other Parts Discussed in Thread: HALCOGEN
Hi All,
I investigate the workaround for this HET PWM issue (HET Issue: Cannot stop pwm output, if duty cycle was set to 100%).
The following is the code of the pwmSetDuty() function generated by HALOCGEN(v04.07.00).
void pwmSetDuty(hetRAMBASE_t * hetRAM, uint32 pwm, uint32 pwmDuty)
{
uint32 action;
uint32 pwmPolarity =0U;
uint32 pwmPeriod = hetRAM->Instruction[(pwm << 1U) + 42U].Data + 128U;
pwmPeriod = pwmPeriod >> 7U;
if(hetRAM == hetRAM1)
{
pwmPolarity = s_het1pwmPolarity[pwm];
}
else
{
}
if (pwmDuty == 0U)
{
action = (pwmPolarity == 3U) ? 0U : 2U;
}
else if (pwmDuty >= 100U)
{
action = (pwmPolarity == 3U) ? 2U : 0U;
}
else
{
action = pwmPolarity;
}
hetRAM->Instruction[(pwm << 1U) + 41U].Control = ((hetRAM->Instruction[(pwm << 1U) + 41U].Control) & (~(uint32)(0x00000018U))) | (action << 3U);
hetRAM->Instruction[(pwm << 1U) + 41U].Data = (((pwmPeriod * pwmDuty) / 100U) << 7U) + 128U;
}
In the last two lines, the PWM duty cycle is set using MOV64 instruction of HET.
The duty cycle is set to 0% and 100% using action=0(CLEAR) or action=2(SET) of MOV64 instruction.
When command duty cycle is 0%, The MOV64 instruction cannot switch PWM output high to low using action=2(SET).
Therefore I modify the code as follows to check action-field of the MOV64 instruction in HET-RAM and use action=3(PULSEHI) instead of action=2(SET) when command duty cycle is 0%.
if (pwmDuty == 0U)
{
if ((uint32)(((hetRAM->Instruction[(pwm << 1U) + 41U].Control) & ((uint32)(0x00000018U))) >> 3U) == 2U)
{
action = pwmPolarity;
}
else
{
action = (pwmPolarity == 3U) ? 0U : 2U;
}
}
I checked the operation using TMS570LS0432 LaunchPAD and the PWM duty cycle switched from 100% to 0% correctly.
Is there a problem with the operation of the MCU using this workaround?
Please teach me if there are any other solution.
Thank you,