Other Parts Discussed in Thread: HALCOGEN
Hello,
I am using the pwm generation on the TMS570 platform using the HET module. I generate the code using HAlcogen (version 03.03.01).
The pwm generation works so far, however if Ithe duty cycle was set before to 100% (pwmSetDuty()) , calling the method pwmstop from the generated het.c does not deactivate the output.
For any other pwm duty cycle, I can stop the pwm generation, and the output on my pin is low.
Should I explicitely set the pin to low, after having called the pwmStop method ?
Thanks an regards
Emmanuel