Part Number: LAUNCHXL2-RM57L
Tool/software: Code Composer Studio
Hello everyone,
I want to connect my Launchpad with CPU but after disconnecting it from the UART serial USB cable, I am not being able to connect it to any CPU.
I have tried to verify its connection but it is also not appearing neither in CCS nor in device manager.
The drivers are installed in the CPU, but still is not being able to read the launchpad.
The power on LED of 5V turns on but the launchpad does not connects.
After removing UART cable, the current limiting LED was on for 10 seconds. After that, the whole launchpad died.
Here is a picture of the launchpad.
P.S. On doing short circuit test, I found out that 3.3V and GND are shorted. Can you please help me to identify where the problem could have occurred?
Anxiously waiting for your response.
Regards,