Part Number: TMS570LS0232
When does this issue occur:
First, the Notification is configured:
Then, the header file containing the correpsonding declaration is configured:
A) The content of the generated files Spi_PBcfg.c and Fls_30_Spi01_Cbk.h do not fit together which leads to the compiler error:
Compiling file: GenData/src/Spi_PBCfg.c
"GenData/src/Spi_PBcfg.c", line 118: error: declaration is incompatible with "void Fls_30_Spi01_DrvSequenceCbk(void)"
(declared at line 37 of "../coremsr/bsw/fls_30_spi01/Fls_30_Spi01_Cbk.h")
B) Not configuring the Notification Header leads to the warning
Compiling file: GenData/src/Spi_PBCfg.c
"GenData/src/Spi_PBcfg.c", line 1234: warning: a value of type "int (*)()" cannot be used to initialize an entity of type "void (*)(void)"
Two possible solutions for this issue:
1. Optionally configuring the notifications header Fls_30_Spi01_Cbk.h and manually adapting the generated declaration. This is not a good solution because, after regenerating the file, the adaption must be done again.
2. Configuring the header and deleting the unnecessary declaration from Spi_PBcfg.c
Would you please comment on that?
Please find the results of the two different configuration options A) and B) as well as the two solution options 1. and 2. in the attachment: