Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN, DP83640
I configured the pin as fallowing :
pinMuxReg->PINMMR0 = PINMUX_BALL_C3_I2C_SCL | PINMUX_BALL_B2_I2C_SDA;
pinMuxReg->PINMMR1 = PINMUX_BALL_E3_HET1_11 | PINMUX_BALL_E5_EMIF_DATA_4 | PINMUX_BALL_F5_EMIF_DATA_5;
pinMuxReg->PINMMR2 = PINMUX_BALL_C1_GIOA_2 | PINMUX_BALL_G5_EMIF_DATA_6 | PINMUX_BALL_E1_GIOA_3 | PINMUX_BALL_B5_GIOA_5;
pinMuxReg->PINMMR3 = PINMUX_BALL_K5_EMIF_DATA_7 | PINMUX_BALL_H3_GIOA_6 | PINMUX_BALL_L5_EMIF_DATA_8;
pinMuxReg->PINMMR4 = PINMUX_BALL_M1_GIOA_7 | PINMUX_BALL_M5_EMIF_DATA_9 | PINMUX_BALL_V2_HET1_01 | PINMUX_BALL_U1_HET1_03;
pinMuxReg->PINMMR5 = PINMUX_BALL_K18_HET1_0 | PINMUX_BALL_W5_HET1_02 | PINMUX_BALL_V6_HET1_05 | PINMUX_BALL_N5_EMIF_DATA_10;
pinMuxReg->PINMMR6 = PINMUX_BALL_T1_HET1_07 | PINMUX_BALL_P5_EMIF_DATA_11 | PINMUX_BALL_V7_HET1_09 | PINMUX_BALL_R5_EMIF_DATA_12;
pinMuxReg->PINMMR7 = PINMUX_BALL_R6_EMIF_DATA_13 | PINMUX_BALL_V5_MDCLK | PINMUX_BALL_W3_SCIRX | PINMUX_BALL_R7_EMIF_DATA_14;
pinMuxReg->PINMMR8 = PINMUX_BALL_N2_SCITX | PINMUX_BALL_G3_MDIO | PINMUX_BALL_N1_MIBSPI1NCS_4 | PINMUX_BALL_R8_EMIF_DATA_15;
pinMuxReg->PINMMR9 = ((~(pinMuxReg->PINMMR9 >> 18U) & 0x00000001U ) << 18U) | PINMUX_BALL_R9_ETMTRACECLKIN | PINMUX_BALL_W9_MIBSPI3NCS_5 | PINMUX_BALL_V10_MIBSPI3NCS_0 | PINMUX_BALL_J3_MIBSPI1NCS_3;
pinMuxReg->PINMMR10 = PINMUX_BALL_N19_RMII_RX_ER | PINMUX_BALL_N15_EMIF_DATA_3 | PINMUX_BALL_N17_EMIF_nCS_0 | PINMUX_BALL_M15_EMIF_DATA_2;
pinMuxReg->PINMMR11 = PINMUX_BALL_K17_EMIF_nCS_3 | PINMUX_BALL_M17_EMIF_nCS_4 | PINMUX_BALL_L15_EMIF_DATA_1 | PINMUX_BALL_P1_RMII_RXD_0;
pinMuxReg->PINMMR12 = PINMUX_BALL_A14_RMII_RXD_1 | PINMUX_BALL_K15_EMIF_DATA_0 | PINMUX_BALL_G19_MIBSPI1NENA | PINMUX_BALL_H18_MIBSPI5NENA;
pinMuxReg->PINMMR13 = PINMUX_BALL_J18_RMII_TXD_0 | PINMUX_BALL_J19_RMII_TXD_1 | PINMUX_BALL_H19_RMII_TXEN | PINMUX_BALL_R2_MIBSPI1NCS_0;
pinMuxReg->PINMMR14 = PINMUX_BALL_E18_HET1_08 | PINMUX_BALL_K19_RMII_REFCLK | PINMUX_BALL_D17_EMIF_nWE | PINMUX_BALL_D16_EMIF_BA_1;
pinMuxReg->PINMMR15 = PINMUX_BALL_C17_EMIF_ADDR_21 | PINMUX_BALL_C16_EMIF_ADDR_20 | PINMUX_BALL_C15_EMIF_ADDR_19 | PINMUX_BALL_D15_EMIF_ADDR_18;
pinMuxReg->PINMMR16 = PINMUX_BALL_E13_EMIF_BA_0 | PINMUX_BALL_C14_EMIF_ADDR_17 | PINMUX_BALL_D14_EMIF_ADDR_16 | PINMUX_BALL_E12_EMIF_nOE;
pinMuxReg->PINMMR17 = PINMUX_BALL_D19_HET1_10 | PINMUX_BALL_E11_EMIF_nDQM_1 | PINMUX_BALL_B4_RMII_CRS_DV | PINMUX_BALL_E9_EMIF_ADDR_5;
pinMuxReg->PINMMR18 = PINMUX_BALL_C13_EMIF_ADDR_15 | PINMUX_BALL_C12_EMIF_ADDR_14 | PINMUX_BALL_M2_GIOB_0;
pinMuxReg->PINMMR19 = PINMUX_BALL_E8_EMIF_ADDR_4 | PINMUX_BALL_B11_HET1_30 | PINMUX_BALL_E10_EMIF_nDQM_0 | PINMUX_BALL_E7_EMIF_ADDR_3;
pinMuxReg->PINMMR20 = PINMUX_BALL_C11_EMIF_ADDR_13 | PINMUX_BALL_C10_EMIF_ADDR_12 | PINMUX_BALL_F3_HET1_17 | PINMUX_BALL_C9_EMIF_ADDR_11;
pinMuxReg->PINMMR21 = PINMUX_BALL_D5_EMIF_ADDR_1 | PINMUX_BALL_C8_EMIF_ADDR_10 | PINMUX_BALL_C7_EMIF_ADDR_9;
pinMuxReg->PINMMR22 = PINMUX_BALL_D4_EMIF_ADDR_0 | PINMUX_BALL_C5_EMIF_ADDR_7 | PINMUX_BALL_C4_EMIF_ADDR_6 | PINMUX_BALL_E6_EMIF_ADDR_2;
pinMuxReg->PINMMR23 = ((~(pinMuxReg->PINMMR5 >> 1U) & 0x00000001U ) << 8U) | ((~(pinMuxReg->PINMMR5 >> 9U) & 0x00000001U ) << 16U) | ((~(pinMuxReg->PINMMR5 >> 17U) & 0x00000001U ) << 24U) | PINMUX_BALL_C6_EMIF_ADDR_8;
pinMuxReg->PINMMR24 = ((~(pinMuxReg->PINMMR4 >> 17U) & 0x00000001U ) << 0U) | ((~(pinMuxReg->PINMMR4 >> 25U) & 0x00000001U ) << 8U) | ((~(pinMuxReg->PINMMR20 >> 17U) & 0x00000001U ) << 16U) | ((~(pinMuxReg->PINMMR8 >> 9U) & 0x00000001U ) << 24U);
/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
pinMuxReg->PINMMR25 = ((~(pinMuxReg->PINMMR12 >> 17U) & 0x00000001U ) << 8U) | ((~(pinMuxReg->PINMMR7 >> 9U) & 0x00000001U ) << 16U) | ((~(pinMuxReg->PINMMR0 >> 26U) & 0x00000001U ) << 24U);
/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
pinMuxReg->PINMMR26 = ((~(pinMuxReg->PINMMR0 >> 18U) & 0x00000001U ) << 0U) | ((~(pinMuxReg->PINMMR9 >> 10U) & 0x00000001U ) << 8U) | PINMUX_BALL_W6_MIBSPI5NCS_2 | PINMUX_BALL_T12_MIBSPI5NCS_3;
pinMuxReg->PINMMR27 = PINMUX_BALL_E19_MIBSPI5NCS_0 | PINMUX_BALL_B6_MIBSPI5NCS_1 | PINMUX_BALL_E16_MIBSPI5SIMO_1 | PINMUX_BALL_H17_MIBSPI5SIMO_2;
pinMuxReg->PINMMR28 = PINMUX_BALL_G17_MIBSPI5SIMO_3 | PINMUX_BALL_E17_MIBSPI5SOMI_1 | PINMUX_BALL_H16_MIBSPI5SOMI_2 | PINMUX_BALL_G16_MIBSPI5SOMI_3;
pinMuxReg->PINMMR29 = PINMUX_BALL_D3_SPI2NCS_1;
PINMUX_GATE_EMIF_CLK_ENABLE(ON);
PINMUX_GIOB_DISABLE_HET2_ENABLE(OFF);
PINMUX_ALT_ADC_TRIGGER_SELECT(1);
PINMUX_ETHERNET_SELECT(RMII);
/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
PINMUX_SET(0,A5,GIOA_0);
PINMUX_SET(18,A11,HET1_14);
PINMUX_SET(3,B3,HET1_22);
PINMUX_SET(1,C2,GIOA_1);
PINMUX_SET(21,K2,GIOB_1);
/*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
PINMUX_SET(0,W10,GIOB_3);
we are using an 50M CLK as an input for ref_clk and the phy is linked as fallowing: 
Have I already in the RMII mode ?
But the
thread i see "We *should* be able to add a pullup resistor to a DNP location on the HDK and make it work in RMII mode. "
Is that means we should pullup some pin of tms570ls3137 like GMII_SEL or anything else?(Value of pinMuxReg->PINMMR29 is 0x01000002)
My problem is I can read and write regs in PHY with MDIO,
I can send data to the RMII(I can see the signal on the rmii_tx0 rmii_tx1 pin), I got the tx interrupt
But I can not receive any data from RMII (I can see the signal on the rmii_rx0 rmii_rx1 pin), I got no rx interrupt
It seems the signal can meets the requirement of tms570ls3137.
When enable the emac loopback option I got tx and rx interrupt.
Is it because I'm not in the RMII mode?
Any other point I can check for this issue? My project is generated by HALCOGEN
Thanks anyone HELP?