Hi,
I have a question about the SAC module built into the MSP430FR2355.
(1) Is it possible to use the SAC module as a "constant current source" in General Purpose mode?
Specifically, I want to output 600 μA.
(2) Is the output of SAC1 directly connected to the ADC (without going through a comparator)?
From the data sheet "6.10.17 Cross-Chip Interconnection (SACx are MSP430FR235x Devices Only)", SAC1 and SAC0 appear to be connected to the ADC via a comparator.
In other words, is the following circuit configuration possible?
Thanks,
Koki