Part Number: MSP-EXP430FR2355
Using ti cloud agent i can debug the project in ccs cloud but in gui code composer serial port not detected for target device
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430FR2355
Using ti cloud agent i can debug the project in ccs cloud but in gui code composer serial port not detected for target device
Hi Dinesh,
In order to connect via the UART, you need to flash the executable on the Launchpad. Are you using this GUI Composer code example?
BR,
Leo
Hi Leo,
yes i tried with example code.when i open in gallery i can run the code and serial port get connected. refer image below

when ever i import to gui composer after run the code serial port didn't get connected to target device . refer image below
Thank you,

Hi Dinesh,
Just to confirm:
1. You downloaded the project for the FR2355 Launchpad and built this with Code Composer to Flash the Launchpad successfully?
2. When you disconnect and reconnect the launchpad, you can see a UART device in your device manager?
Which version of Code Composer did you use?
BR,
Leo
Hi Leo,
1.yes,i can flash the code successfully.
2.yes,i can see the uart device in UART MANAGER
Version: 10.3.1.00003 code composer i am using.
Hi Dinesh,
Can you provide the link to the CCS project you are building/flashing? Is this from resource explorer? I want to make sure you are building the project that corresponds to the GUI you are trying to connect with.
BR,
Leo
Hi Dinesh,
From within the GUI project can you try downloading the firmware to your Launchpad as indicated below?
BR,
Leo
Hi Dinesh,
It looks like you are having an internet connection problem. I have tried going to the GUI here:
https://dev.ti.com/gallery/view/3491167/MSP-EXP430FR2355_OOB_GUI/ver/1.0.2/
and it successfully downloaded to the Launchpad on my side. Is your internet connection through a corporate network?
BR,
Leo
Hi Dinesh,
It's not clear to me why you're not able to connect to the cloud agent. Are you using Chrome? (I tested with Chrome here.)
BR,
Leo
yes leo, i am using chrome but its working perfetly with ccs cloud in that i can debug the program using ti cloud agent.
only in gui facing this issues
Hi Dinesh,
Can you check the jumpers on your Luanchpad? There are two jumpers labeled RXD/TXD that have to be populated. Do you have more than one Launchpad? Can you confirm that the project that you built and flashed to the platform is this one?
BR,
Leo

https://dev.ti.com/gallery/view/3491167/MSP-EXP430FR2355_OOB_GUI/ver/1.0.2/
yeah,from above link i can flash the program to launch pad and run .
only problem i have was while importing project iam unable to connect with target device you can refer below link for importing project and i have only one launch pad
https://dev.ti.com/gc/preview/default/MSP-EXP430FR2355_OOB_GUI/index.html
Hi Dinesh,
I have to conclude that if you can flash the program but can't connect via UART(after resetting the Launchpad) that there must either be some hardware problem with your Launchpad - or some configuration on your computer which is keeping GUI composer from connecting over the UART. You might try connecting to the Launchpad with a terminal emulator and send it some commands to rule out a problem with the Launchpad.
BR,
Leo
Hi Leo,
No while i run example code in gallery it works perfectly,only when i import example code to my projects in gui composer unable to flash program,unable to connect to serial port.
**Attention** This is a public forum