Part Number: MSP430FR6989
Hello
I'm really stuck with very strange errors when migrating from STM8L , like:
#170 a function type is not allowed here
in header files, which is very strange. Where else should it be then?
or
#102 "GetCurrentFlow" has already been declared in the current scope
but it never was and so on.
I think I've added header files correctly
#81 storage class may not be specified here
Where can I find a manual that has these errors listed? I only came across 'MSP430 Optimizing C/C++ Compiler" which is about optimizing as stated.