This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2100: Enabling and utilizing the internal 1.5V reference for ADC measurement

Part Number: MSP430FR2100


I am trying to utilize the internal 1.5V reference as my ADC voltage reference. First, I enable the reference by setting:

PMMCTL2 = REFBGEN+REFGEN+INTREFEN;

Then I wait for the REFBGRDY and REFGENRDY to go high, which they do.

For the ADC settings, I am selecting ADCSREFx = 001b in ADCMCTL0 (utilize VREF as Vr+)

Now, when I measure a 1.0V input, I am getting all 0x3ff (all 1's) for my conversion result, which is incorrect.

I have been able to successfully measure the 1.0V input using ADCSREFx = 000b (utilize AVCC as Vr+), so I am confident that my ADC settings are correct.

As an experiment, I set ADCSREFx = 000b and then measured Channel 13, which should return the measurement of the 1.5V reference, but I got all zeros.

So it appears my 1.5V reference is not generating the voltage. How can I enable it?

**Attention** This is a public forum