Part Number: MSP430FR2532
Other Parts Discussed in Thread: MSP-FET
Hi,
I have the problem, that the µC wouldn't start run the application after I load the reset vector address in the PC. Communication is over UART. When I reset the device with the RST pin everything is fine, but the circumstance doesn't allow me to control this pin. So in my thoughts it should be possible to use the Load PC command and invoke the reset vector address 0xFFFE into the PC to reset the device after I finished the download via BSL.
When I stop the device in debug mode (using IAR EW) after I use the Load PC command, the controller is here (BP not active):

and I can't go further by clicking Go (F5).
When I activate the breakpoint at 0xFFFE the controller is here:

and after I click Go (F5), the application is running.
Any suggestions why the controller does no reset? Without the MSP-FET I got an ACK from the BSL after I send the Load PC command and the controller also doesn't run the application. I think it is the same behavior as I mentioned first.