This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2476: GPIO digital Input not capturing every interrupt

Part Number: MSP430FR2476

I am using MSP430fr2476 micro-controller for capturing low to high pulse using P6.1

If the input voltage is greater than 4.1 v with DVCC as 3.4 V than what can happen to P6.1 Digital Input

Is there any possibility that it will miss capturing the interrupt?

With Regards,

AD

**Attention** This is a public forum