Part Number: MSP430FR5962
So far I've tried optimization levels 0 and 1 and played around with --opt_for_speed with no success. Currently optimization level 2 seems to work for some reason, but so did -o1 until I eventually had the same issue. What happens is the compiler seems to pick a function at random (it seems to be a new one every time there's any code changes) to optimize out. Disabling optimization completely solves the issue.
A call to the optimized out function leads me to an address containing all BRA @PC instructions, which of course sets my PC to 0 and the program remains halted.
I should also note that my FRAM2 is 100% full, with FRAM at 82% and RAM at 81%.