Part Number: MSP430FR5962
Hi all Experts,
I'm working to create a custom code where I want a separate bootloader and separate application code memory. So I have defined the memory for Bootloader as well as application memory. My linker file looks like this
-P(CODE)BOOT_MEM=4000-5FFF
-P(CODE)APP_MEM=6000-BFFF
-P(CODE)CODE=4000-FF7F,10000-23FF7
-Z(CODE)CODE_PAD
Here in the linker file, I have defined Booloader memory as 4000-5FFF and for Application memory, it is 6000-BFFF. I'll also attach my code for reference just to get feedback on whether my approach is correct.
One more thing I would like to mention is that for bootloader I'm creating a different project and for application memory, it's a different project itself.
#include <MSP430FR5969.h>
#include <stdio.h>
#include <stdint.h>
#include <stdbool.h>
#pragma location="INFOA"
int application_memory;
#pragma location="COPY"
void check_app_flag()@ "COPY"
{
if(application_memory == 1)
{
for(int l = 0; l<30; l++)
{
P1OUT ^= BIT0;
__delay_cycles(50000);
}
}
}
#pragma location= "APPLICATION_MEMORY"
void main( void )@ "APPLICATION_MEMORY"
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
int l;
P1OUT &= ~0x01;
P1DIR |= 0x01;
PM5CTL0 &= ~LOCKLPM5;
check_app_flag();
for(l = 0; l<10; l++)
{
P1OUT ^= BIT0;
__delay_cycles(800000);
}
for(l=0; l<15; l++)
{
P1OUT ^= BIT0;
__delay_cycles(100000);
}
application_memory = 1;
// Force a Software BOR
PMMCTL0 = PMMPW | PMMSWBOR;
}
#include <MSP430FR5969.h>
#include <stdio.h>
#include <stdint.h>
#include <stdbool.h>
#pragma location="INFOA"
int application_memory;
#pragma location="COPY"
void check_app_flag()@ "COPY"
{
if(application_memory == 1)
{
for(int l = 0; l<30; l++)
{
P1OUT ^= BIT0;
__delay_cycles(50000);
}
}
}
#pragma location= "APPLICATION_MEMORY"
void main( void )@ "APPLICATION_MEMORY"
{
// Stop watchdog timer to prevent time out reset
WDTCTL = WDTPW + WDTHOLD;
int l;
P1OUT &= ~0x01;
P1DIR |= 0x01;
PM5CTL0 &= ~LOCKLPM5;
check_app_flag();
for(l = 0; l<10; l++)
{
P1OUT ^= BIT0;
__delay_cycles(800000);
}
for(l=0; l<15; l++)
{
P1OUT ^= BIT0;
__delay_cycles(100000);
}
application_memory = 1;
// Force a Software BOR
PMMCTL0 = PMMPW | PMMSWBOR;
}