Other Parts Discussed in Thread: MSP430F5438
My question has to do with the decoupling capacitor network for the digital Vcc on this uC. 10 uF in parallel with 0.1 uF is recommended, but there are 4 power and ground pins for the digital power input (DVcc & DVss). So should I divide the capacitance by the number of pins (4) and locate 4 parts of each value around the perimeter of the uC or just use a single part for each one recommended?