This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2121: MSP430F2121 Programming - Reg

Part Number: MSP430F2121
Other Parts Discussed in Thread: MSP430FR5870, MSP-FET, MSP-FLASHER

Dear Team,

We have used MSP430F2121 and MSP430FR5870 MCUs in our Products. Currently MSP-FET is being used to Program the MCUs during development.

Can the same programmer/debugger be used in Production environment or any other programmer is recommended for reliable and quick programming.

Quantity of boards programmed will be around 1K to 2K per day. 

With Best Regards,

B.Saravana Vikram.

  • MSP-FET is not recommended for this, but it can be used (in combination with open source CLI MSP-Flasher) if high speed programming is not priority, and handling one-by-one target device is enough.

    MSP-GANG is made for this. It can work standalone (without PC) it is fast and can do 8 devices in parallel. However there is no CLI for PC side only GUI and scripting option, working only on Windows (no Linux or OS X).

**Attention** This is a public forum