Part Number: MSP430F5659
Other Parts Discussed in Thread: MSPBSL
We need to modify one of the USB bootloaders because we are using a non-standard clock crystal but it does not appear that the source for the specific variant we are using is available, although the binary files are available.
We have tested and used the bootloader provided in MSP430BSL_1_02_00_01\Released_BSL_Images\MSP430F665x_Family\USB BSL as part of the “MSPBSL_CustomBSL430_1_02_00_01” package. This works on one of our boards where we replaced our clock with a 34mHz clock. In the same package there is an IAR project for the MSP430F552x series, but not our device family “MSP430BSL_1_02_00_01\IAR_BSL_Source\IAR_v6_MSP430F552x_USB”. Do you know if the source project for the MSP430F665x Family code is available?
if you can point me in right direction that would be much appreciated