Hi TI,
In our mspg2553 we are using using UART at pin p1.1 and p1.2 and p2.3 as an input pin. uart communication is working well, while input at gpio p2.3 is low but while it is high. uart communication is getting disturb. I mean communication is going slow and receiving invalid data.
here is my code, please have a look and let me know if anything is wrong.
Uart Initialization:
UCA0CTL1 |= UCSSEL_2; // SMCLK
UCA0BR0 = 104; // 16MHz 9600
UCA0BR1 = 0; // 16MHz 9600
UCA0MCTL = UCBRS_0 + UCOS16 + UCBRF_3; // Modulation UCBRSx = 0
UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine**
IFG2 &= ~(UCA0RXIFG);
IE2 |= UCA0RXIE; // Enable USCI_A0 RX interrupt
GPIO :
void initGPIO()
{
P1DIR |= BIT0; // DE_RE pin Mode as OUTPUT
P2DIR |= BIT4; // B_Led pin Mode as OUTPUT
P2DIR |= BIT5; // C_Led pin Mode as OUTPUT
P2DIR |= BIT6; // D_Led pin Mode as OUTPUT
P2DIR |= (BIT1 + BIT2); //(P2.0-DoorLockOperator_A and P2.2 Fan operator)as output
P2SEL &= ~(doorLockStatus_A); // i/o function selected, 0
P2DIR &= ~(doorLockStatus_A); // P1.5 as input
P2OUT &= ~(doorLockStatus_A); // select pull-down mode
P2REN |= (doorLockStatus_A); // Enabling Pull Down Resister
P1OUT &= ~BIT0; // DE_RE initially Low/receiving mode
P2OUT &= ~BIT4; // B_Led LOW Initially/OFF
P2OUT &= ~BIT5; // C_Led LOW Initially/OFF
P2OUT &= ~BIT6; // D_Led LOW Initially/OFF
P2OUT &= ~BIT0; //DoorLockOperator_A LOW Initially/OFF
P2OUT &= ~BIT1; //Optional LOW Initially/OFF
P2OUT &= ~fanOperator; //FAN Operator LOW Initially/OFF
P1SEL |= BIT3; // ADC input pin P1.3
P1SEL = BIT1 + BIT2; // P1.1 = RXD, P1.2=TXD
P1SEL2 = BIT1 + BIT2;
}
where door lock pin is
#define doorLockStatus_A BIT3 // P2.3===>P2.0
apart from this i have one ADC pin as well, but i think that doesn't matter:
// Function containing ADC set-up
static void ConfigureADC()
{
ADC10CTL1 = INCH_3 + ADC10DIV_3; // Channel 3, ADC10CLK/3
ADC10CTL0 = SREF_0 + ADC10SHT_3 + ADC10ON + ADC10IE; // Vcc and Vss as reference, Sample and hold for 64 Clock cycles, ADC interrupt enable
ADC10AE0 |= BIT3; // ADC input enable P1.3
}
do let me know if anything is wrong.
thanks
sarju