Part Number: MSP430F5529
Hi all,
I just inherited an ongoing project. I think it was developed in 2016.
Code is for msp430f5529-based board. It is currently running, working and selling.
I have been able to import it to CCS10.x. It was developed for CCS6 but, as long as I have the proper tools versions, I don't think this is gonna be a problem
I was able to install its TI-RTOS 2.20.0.06 dependency as long as a v18.x compiler (required v15.x).
However, I reached a point I cannot solve the compilation "error #41 expected an identifier".
It takes me to file msp430f5529.h, line 3707.
SFR_8BIT(USBIEP0BUF); /* Input endpoint_0 buffer */ SFR_8BIT(USBOEP0BUF); /* Output endpoint_0 buffer */
When ctrl+clicking the USBIEP0BUF word, it takes to file defMSP430USB.h, line 178
//input and output buffers for EP0 #define USBIEP0BUF 0x2378 #define USBOEP0BUF 0x2370
When ctrl+clicking the macro definition, it opens a file dialog

Any idea is appreciated Of course, feel free to ask about any other info you may require.